Part Number: LMP8603-Q1
Hello,
I would like to use the LMP8603-Q1 current sense amplifier in a system which has a variable current range (0~25mA, -1.5A~1.5A). I would like to use the ability to reduce the gain by switching in the resistor from A1/A2 to ground. For the lower current range 0~25mA, it will keep the resistor disconnected so the gain is 100. For the higher current range -1.5A~1.5A, it will connect a 2.7kOhm resistor which should drop the gain to ~2.6 if my calculations are correct.
Is there any issue using the current sense amplifier in this way?