This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8329EVM: EVM is not connected

Part Number: MCF8329EVM

Even after powering of EVM device with 12V it is still showing EVM is not connected.
image.pngDK_INVOICE_126966394.pdf 

  • Hi Vinay,

    Please confirm that the R47 potentiometer is positioned correctly and verify the voltage measurement on the speed/wake pin located at connector J9. This pin should show 3.3V.

     

    Thanks,

    Dhinesh