This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7171: LM7171 Oscilation

Part Number: LM7171

LM7171 oscilates at 28MHz.

Netlist is as following.

According to the datasheet, would it be better to place a 2pF Capacitor in parallel with the 820ohm resistor between 2 and 6, or change the 10ohm output isolation resistor between 6 and 13 to 50ohm?

2 3 4 6 7 LM7171

IN 3 820ohm     2 6 820ohm     6 13 10ohm     6 12 1kohm     7 GND 0.01uF     7 GND 1uF

7 GND +15V     4 GND 0.01uF     4 GND 1uF     4 GND -15V

12 13 14 17 16 AD847 (Next Stage)

12 16 1kohm     12 16 1pF     17 GND 0.1uF    17 GND +15V     14 GND 0.1uF

14 GND -15V