This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1311: AMC1311 for measuring AC power line

Part Number: AMC1311
Other Parts Discussed in Thread: AMC3330

I am using AMC1311 for a sensor that was used to measure the power line. The low side of AMC1311 was fed into an adc pin to a TI microcontorller. 

  1. assume I use AC power line for input, 120v, 60Hz. I assume the peak could be 170v. 
  2. I use a 1M ohm and 10k ohm for divider, and voltage from 10km is fed into pin2 of AMC11311
  3. pin3 and pin4 are connected to the negative of power line. 

My question is: Is this design OK? Do I need to add a rectifier? some people told me I don't need. 

sorry for this easy question. I am not EE, and just started to solve this problem.