AMC1350: Absolute Maximum Ratings

Part Number: AMC1350

I have a question about the input voltage of the AMC1350.

It is specified as ±5 V input, but the absolute maximum ratings (P4) list MIN: -15 V and MAX: 15 V.

If a noise spike exceeds ±5 V even for a single pulse, could that cause damage?

I would appreciate your response.