Part Number: INA133
The INA133U amplifier was discontinued and recommended to be replaced by INA133U/2K5. My system has a requirement for operation down to -54°C which the original part was rated to, but the replacement part is not. Is the INA133U/2K5 tested down to -54°C, and if so, can that test data be provided? If it is not tested down to that temperature, is there another drop-in part that could replace INA133U? Thanks.