Part Number: TAS2563
According to the datasheet, the amplifier consumes around 4 mA from VBAT and 11–12 mA from VDD during active operation, resulting in approximately 15–16 mA per amplifier. With two amplifiers in stereo mode, we observe around 30–32 mA total active current. Is this the expected behavior?
We know disabling the I/V sense can reduce the current by about 2 mA per amplifier. Are there any other settings or recommendations to significantly reduce the active current, such as lowering the boost voltage (e.g., from 12 V to 6 V) or other power optimization options? Is there Any Blocks I can Disable to reduce VDD power