This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2381: Clocking

Part Number: OPA2381
Other Parts Discussed in Thread: OPA381

Hi Team,

I am currently working on another project for Zeiss where they use OPA2381. They thoroughly investigate on temperature behavior and they have found a kind of resonance with some OPAMPs. Do the two Opamps within the package share the same clock?

Thanks,

Federico

  • I do not believe the two channels of OPA2381 share the clock but even if they had it is highly unlikely to show as resonance "with some Op Amps" - please show the scope image. The OPA381 series op amps use an auto-zero topology with a time-continuous 18MHz op amp in the signal path. This amplifier is zero-corrected every 100µs using a proprietary technique. Upon power-up, the amplifier requires approximately 400µs to achieve specified VOS accuracy, which includes one full auto-zero cycle of approximately 100µs and the start-up time for the bias circuitry. Prior to this time, the amplifier will function properly but with unspecified offset voltage. This design has virtually no aliasing and low noise. Zero correction occurs at a 10kHz rate, but there is virtually no fundamental noise energy present at that frequency due to internal filtering. For all practical purposes, any glitches have energy at 20MHz or higher and are easily filtered, if necessary. Most applications are not sensitive to such high-frequency noise, and no filtering is required