Part Number: THS3470
I am using the THS3470 as a pulse amplifier and because of the input common mode range of (Vee + 4) I have a -5 V bias on VEE and 50 V on Vdd. Are there any considerations I should be aware of.
I also see in a post a while back that the current monitor should be connected to Vmid when using unequal supplies. I am currently using the EVM which ties the Imon to ground via a 1K resistor. Will this cause issues monitoring the current?