Other Parts Discussed in Thread: ADS1298
I am interested in building a precision AC current source that can accurately generate 200nA p-p of AC current. Not sure yet if I want a DC current of 50nA to allow single supply operation, but I can power this off either a single +3.3V supply or +/-3.3V. Can anyone help me with this or guide me in the right direction? Thanks. The frequencies I want to generate are 1Hz, 10Hz, 40Hz, 100Hz, 500Hz, and 1KHz.