THS4552: Higher Absolute part

Part Number: THS4552
Other Parts Discussed in Thread: THS4561, THS2630

Dear Team,

My customer has used the THS4552IRTWR with Vs+=5.0V in their system.
However, there are concerns about Vs+ higher than 5.5V in their system.
However, Absolute maximum rating of Vs+ of the THS4552 is 5.5V (max).
Do you have a device with the same characteristics as the THS4552 with the absolute maximum rating of 6.0V?

Best Regards,

Koshi Ninomiya

  • Hi Koshi,

    Does the customer require a dual channel amp for their use? Unfortunately, we do not have any dual channel's that are rated for above 6 V. If single channel is okay, the THS4561 and the THS2630 both fit the voltage supply requirements. The THS4561 is a bit slower with around the same slew rate, while the THS2630 is faster with a slower slew rate. Let me know if there are more specifics about what the customer needs and I can help narrow down more parts!

    Best,

    Lukas