Other Parts Discussed in Thread: INA129, INA826, TINA-TI
Hi,
I'm attempting to amplify a signal from a Hall effect Current Sensor with an INA129. Over the range 0-30A the sensor outputs 2.5 - 3.7V. I have this output connected to the Vin+ input of the amp and a 2.5V connected to the Vin- input. The 2.5V comes from a regulated 5V voltage divided by 2. The amp is single supply powered with 24V.
I want to have a 0-10 V output across the 0-30A range. I'm currently using a 7K68 Ohm resistor for Rg which would give a Vout of 9V at 30A.
When tested at 25A I am only getting a Vout of 4.1V. I have switched Rg for a 800 Ohm resistor (Gain = 73) and at 25 A I'm getting 4.5V.
I understand that I won't be able to get Vout right down to 0V but is this also affecting the Vout max? If not could you provide some further suggestion including a more appropriate part for the application?
I look forward to your reply.