Part Number: LM358BA
Other Parts Discussed in Thread: LM358B, ISO7762, AMC0311S, ADS7042, ADS8675, AMC0311R, AMC4311R, AMC131M01, ADS7253
Hi,
- Earliesr we used LM224DR 4channel, we need same specification in 2 channel. LM358BA or LM358B can be used to replace LM224DR and keeping the same supporting circuit?
- I want to measure Welding Torch Voltage using simple voltage dvider and need to isolate. Kindly suggest the suitable Isolated Amplifier, we use SPI interface External ADC between Amplifier and MCU.
- Any drawback on Isolated Amplifier? Can we use Isolated Amplifier or we need to use Isolator ISO7762 with ADC, which is best option.
Thanks and regards,
Naveen K