Part Number: INA128
I am not using a gain resistor and leaving the pins unused. I would have expected a gain of 1 but it is actually 1.22. I have grounded the reference pin and I am using + and - power source. Wondering why the gain is not 1.
Part Number: INA128
I am not using a gain resistor and leaving the pins unused. I would have expected a gain of 1 but it is actually 1.22. I have grounded the reference pin and I am using + and - power source. Wondering why the gain is not 1.
Hi Robert,
What are the voltages that you are applying on the input pins?
Also, what supply voltages are you applying?
Best Regards,
Robert Clifton
Hi Robert,
Thanks for replying quickly. I have a few follow up questions:
- The differential voltage between the inputs ranges from 0-2.8V?
- What is the common mode voltage?
- Is this one part that is exhibiting it or multiple?
- If multiple is it all of them or a certain percentage?
Best Regards,
Robert Clifton
I wanted to post the schematic, but I cannot figure out how to do it. I reconfigured the circuit and I will try to explain in words what it looks like. +12 volts at pin 7, -12 volts at pin 4, pin 5 is grounded, +5 volts applied to pin 3, pin 2 grounded. Nothing at pins 1 and 8. This supplies a voltage of 5 volts at the + input with respect to the - input. That would be a common mode voltage of 2.5 volts which is within spec. There is a feedback resistor added from pin 6 to pin 3 of 105K, something the data sheet recommends. (Taking it out had no bearing on the result). For the input described, the output voltage at pin 6 with respect to ground is 6.15 volts, giving a gain of 1.22. I bought seven of these ICs and all test out to give the same result. Thanks.
One thing I should mention is that this is a wire wrap prototype (yes, I still wire wrap). I suppose that if the resistance from pin 5 to ground is not exactly zero then the 40K resistor internally connected to pin 5 would change and possibly upset the gain calculation. However, I ran the numbers out with an additional 8 ohms from pin 5 to ground and it made negligible difference in the gain of the internal differential amplifier.
Hi Robert,
Do you have a resistor going to ground for the non-inverting input pin (pin 3)?
I'm thinking this has something to do with your common mode voltage being very low relatively to the reference pin. I'll see if I can test it in lab to try to recreate your results.
There is a feedback resistor added from pin 6 to pin 3 of 105K, something the data sheet recommends. (Taking it out had no bearing on the result).
I've looked through the datasheet and didn't see this suggestion. Not that it's important since you have confirmed that it's not the problem.
Best Regards,
Robert Clifton
Hi Robert,
I went into lab and tested one of my INA128 devices I had on hand. I couldn't recreate your issue. However, I was getting an output of 3.9V with the setup you described shown below:

To me this looked like a boundary plot issue. What I did to prove this was the case was I raised the voltage seen by both inputs by 2V, making the circuit look like this:

When I did that, the output voltage was producing a 5V signal. This tells me that we were violating the input common mode range.
I'm not sure why your signal is going up to 6.15V but would you be able to create my test to see if your results change?
Best Regards,
Robert Clifton
Hi Robert. I solved the problem today although it was a blunder on my part and the INA128 performs as per the data sheet. I flipped my perf board prototype over and found that I had tacked a 221K resistor across pins 1 and 8. I think I meant for it to go somewhere else. But, if you run the numbers out using their gain equation, it equates to a gain of 1.22. So, problem solved; just carelessness on my part. The resistor was on the bottom of the perf board so I kept overlooking it. Thanks for your time. BC
Hi Robert,
It's quite alright! Glad you were able to find it and fix it.
Best Regards,
Robert Clifton