Part Number: LMH5401
Other Parts Discussed in Thread: ADC3669,
Dear Technical Support Team,
I have a question about the LMH5401 in the ADC3669EVM-DC. The LMH5401 is a dual-supply device operating at 3.5 V and -1.1 V. The signal I want to measure with the ADC is -200 mV, which is amplified 4 times by the LMH5401 (to 800 mV with VCM = 1.4 V) and then fed into the ADC3669. However, a signal of approximately -1 V is periodically applied.
Q1
Can the -1 V signal be ignored as it is clipped due to overdrive? Or should I protect the input from the SMA with a clamping diode?
Q2
What time scale does the “overdrive recovery” value of 300 ps or 400 ps in the datasheet refer to? Is it on the order of a few ns, as stated in the datasheet? If overdrive occurs for a duration of 10 ns or less, will the recovery time be longer?
Q3
Is it acceptable for overdrive to occur periodically as long as it does not exceed the absolute maximum rating?
Best Regards,
ttd