Part Number: INA181
Other Parts Discussed in Thread: TPS63802
Hello,
I would like to confirm a possible failure mechanism with the INA181A1IDBVR.
Setup:
- VS is supplied from an MCU GPIO (3.3 V when on, 0 V when off), with 0.1 uF bypass.
- REF is driven by a DAC (MCP47CVB02) at 0.5 to 1.65 V, and stays driven while VS is off. The DAC can source 6 to 14 mA into a short.
- IN+/IN- sit across a 0.05 ohm high-side shunt at 0 to 5.9 V.
- OUT drives the FB pin of a TPS63802 to regulate LED current.
After some time in the field, one device's output stays at 0 V regardless of sense current.
Questions:
1. With VS = 0 V and REF at 0.5 to 1.65 V, does current flow into REF through an ESD structure to VS, and roughly how much would it be?
2. Can this condition cause latch-up or damage when VS is then applied?
3. Is an output stuck at 0 V consistent with that kind of damage?
4. Would a 1 to 2 kohm series resistor on REF be an acceptable fix, and what effect would it have on gain error and CMRR?
Thank you,
William Deshaies