TLV9004: TLV9004 1.8V operation

Part Number: TLV9004
Other Parts Discussed in Thread: AM2434, TLV9054, TLV9064

Hello,

we intend to use the TLV9004 (or TLV9054, TLV9064) as a volatge follower to drive the ADC of the AM2434.

We plan to power the OPAMP with the 1.8V supply of the AM2434 which has a voltage tolerance of 1.8V +/-1.5%. This also ensures that the voltage specifications of the ADC inputs are not exceeded.

The TLV90x4 is specified from 1.8V to 5.5V, but not from 1.8V-1.5%.

Are there likely to be any problems if we operate the TLV90x4 at 1.8V ±1.5%?