Opening the OPA277 TINA-TI reference circuit revealed a circuit that was virtually unrecognizable-- the previous op amp symbol, which was the same standard symbol used in all the TI/BB op amps has been replaced with a non-standard symbol that has now sprouted trim pins! The size of the new symbol is not compatible with TINA-TI circuits using the standard symbols so it is tedious to have to re-draw the circuit to accommodate this new OPA277 symbol. It is bad enough having to deal with some TI high-speed op amps that are drawn upside-down.
In addition, the reference circuit has been replaced by a circuit that looks like it was cobbled together by a beginner. Was this necessary? Improvements I can understand but this? I have attached the original OPA277 reference circuit (found in the TINA-TI "Examples" - "TI Test Circuits" - "OPA277 Test Circuit.TSC")
Open the one on the current TI OPA277 page and compare the two. Is anyone at TI paying attention to things like this?