Other Parts Discussed in Thread: LM339
Do bias current of opamp flow into inverting & non-inverting terminal? how to determine in which direction current will flow.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Aamir,
It depends. If the data sheet shows a negative IIB then conventional current flows out of the device. If it is positive then current flows into the device.
If the data sheet IIB value shows positive and negative values then the op-amp has bias current cancellation circuitry and the current will be small but the polarity may be either.
PNP input devices have a negative IIB (current flows out of inputs)
NPN input devices have a positive IIB (current flows in to inputs)
Regards,
Ron Michallick
Hi,
Thanks for ur reply.
1. IN NPN, JFET devices current always flows out while in PNP devies always current flows out. Right. Now I think there no exception here. Right?
2. In below diagram, with dual supplies,direction of flow of current is shown, which gives input bias current & error accordingly right.

Now, in case of single supply, as shown below, what is direction of current, I don't understand, what is direction of input bias current here

The input current on a JFET (junction field effect) transistor is based on PN leakage current and is exponentially proportional to temperature.
The OP-AMP in the picture is a LM339 with a PNP (bipolar, not JFET) input and the current flows opposite of your drawn arrow.
In the second setup, the current still out of pins 6&7 (just like the first schematic).
Regards,
Ron
Aamir,
For NPN input stage, current flows as you drew in first picture.
On second picture, there would be no current flow and the op-amp would not work. NPN input op-amps do not support input voltage equal to the negative supply rail.
Regards,
Ron Michallick