Other Parts Discussed in Thread: OPA4209
I am using the OPA4209 as a voltage tracker in my design. Just input signal to the non-inverting input then connect the output and inverting input directly.
For lack of experience,I have two questions.
1. When the Rload is 50r, can the output voltage swings to 1V? I can't find the current output capability in the datasheet, only know the short current and rail-to-rail output. (It can swing to 1V into 50r in the simulation, but I want to make sure)
2. When estimate the output voltage noise of OPA4209, what bandwidth should be used? the 18MHz (the OPA4209 bandwidth,unit gain) or the bandwidth alone the signal path after the OPA4209?