Other Parts Discussed in Thread: THS4504, THS4505, TINA-TI
I am using the THS4504/5 fully differntial amplifier and have a question about the data sheet specification for common mode input range. The common mode input range is pecified for +/-5V power supplies, and is -5.1/+2. This is an overall range of 7.1V. The common mode range is also given for single supply +5V to 0V, and is -0.1 to +2V. If the negative power supply is changed to -8V, does the upper value of the common mode input range also change? Does the 7.1V range shift to -8.1V/-1V or does the upper limit remain constant at 2.1V no matter the negative supply value? It is unclear from the data sheet specifications and TI technical suipport does not seem to know the answer and has directed me here to pose the question.