Other Parts Discussed in Thread: INA149, OPA277, INA117, INA129, OPA2171
Hello
I need to make a current limiting device that senses current and depending on the value of it is controlling the duty cycle of a PWM signal.
My though is to use a differential amplifier or an instrumentation to sense the voltage drop across the sense resistor. Then the output of the amplifier will go to a gain amplifier for amplification. Finally the signal will go to an ADC, the FPGA will read ADC and with some calculation it will produce the PWM signal
Requirements
Common voltage voltage 200volts
Amps sense between 1A and 10A, accuracy is not of top priority
For differential amplifier I’m thinking of using an INA149
The part has max input offset of 1.1mV, so with 1A across a 0.01Ω resistor that’s 10% error, correct? When the Amps increase the error will reduce
The other important parameter is CMRR I have to look at. How can I calculate it for different common voltages?
I have made a draft circuit and I will start building the details later. I want to hear your opinions and suggestions for correct implementation
The Vin will be around 150 Volts not 10