Other Parts Discussed in Thread: PGA308, PGA308EVM
hi,
there is a program that allows the configuration of the PGA308 without the aid of PGA308EVM board?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Claudio,
The PGA308EVM with its included software is the fastest way to get up and running with the PGA308. Communications over the one-wire interface are built-in and running a calibration is simple. It is also possible to use the PGA308EVM software with your own PGA308 board. To do this, you must purchase the PGA308EVM and connect your board to the included USB DAQ Platform. I've attached some PowerPoint slides which show how to do this.
We also offer the PGA308 Multi-Cal system (http://www.ti.com/tool/multi-cal-system) which supports simultaneous calibration of up to 64 PGA308 modules. This tool is well-suited for use in mass production and also includes software to simplify the calibration process.
Best regards,
Ian Williams
Linear Applications Engineer
Precision Analog and Sensing Products
hi Ian,
thanks for the tips, but I don't have the PGA308EVM available in short time and I try to find a faster alternative.