TI Team-
I have a question about how the TLC2264 and the TLC2254 compare. I'm using the precision amp as a buffer amp to the input stage of a 12-bit ADC. I closely examined the datasheet for both devices, and for my particular application I am mostly concerned about the DC specifications.
With the exception of power, offset, and drift, is there anything else I should know about the TLC2264? I'm willing to deal with the larger DC specification, which is fine because the TLC2264 is much harder to purchase via my CM.
Again, my question is as follows:
- I'm using the TLC2254CPW (14 pin SOIC), but I plan to use the TLC2264CPWR as a drop in replacement. Aside from the differences in the DC specification, is there any other reason why I may not want to use this device as a replacement.