Other Parts Discussed in Thread: TLV3501
I have made a TLV3501 PCB as mentioned in the datasheet. I want to test out the PCB before I link it up with my other PCBs. Can someone tell me what tests or equipment I should use? Note that my emphasis is on the accuracy of the PCB and check that the PCB is correct rather than the performance of the PCB.
Additional Info:
I am using this PCB in a communication circuit. It is used in linked with the AD8318 which is an RF detector. Together they detect pulses and provide with a output which is actually a stream of pulses. The pulses occur with a maximum frequency of 5 MHz.