Other Parts Discussed in Thread: XTR111, XTR110
I am using two XTR110s in my product. The span adjust is barely large enough, and has a known interaction with the zero adjust. The zero adjust does not have enough range to make up for some voltage offsets that are created by the amplifers earlier in the circuit. I am using 100K ohm pot on the zero and 100k ohm pot and a 10k ohm resister on the span adjust.
Is there any way to increase the zero adjust range?
Thank you.