Other Parts Discussed in Thread: THS4521, TINA-TI
I'm testing out the THS4521 using the simulation circuit in TINA-TI. I had the PD pin pulled low (to the ground) and the amplifier was still amplifying. I though when the PD pin pulled low it is the same as shutting off power to the amplifier (V+ and V-) and therefore the amplifier is shut off.
Also, if I pulled the PD pin to low (i.e. power down) but Vcc still connected to an active +5V and Vss is grounded can I still apply a larg voltage to the input pins (Vin+ and Vin-) of the amplifier? Specifically, can I apply a sinewave with amplitude of +12Volts (i.e. swings from -12V to +12V) at the Vin+ and a sinewave with 180 degree phase shift from the previous sinewave with amplitude of +12V to -12V to Vin- of the opamp? Will this damage the opamp?
Thank You,
Loc