Other Parts Discussed in Thread: TL084, TINA-TI
I have a question concerning the quiescent state of the TL084 op amp. I have a quad TL084 op amp and I want to know what is the quiescent state voltages of the op amp? Should there be a voltage at the output if I don't have anything connected to the chip except for the Vcc and -Vcc?
I have the op amp connected to +/-12V power supply and nothing connected to either the inverting input, non-inverting input, or the output, but I am getting a voltage of -10.34V on the output.
Also when I do configure the op amp as an inverting op amp with a gain of 10, and a Load Resistance of 2k Ohms, I am getting no voltage swing on the output when I feed the amplifier a signal of 0.5Vp-p. If I load down the output with a Load Resistance of 100 Ohms or less I will get a signal swing but the chip does get rather warm with this kind of load. Any guess as to why the chip acts this way?