Other Parts Discussed in Thread: OPA350
Hi,
I'm looking at an Op Amp design where and OPA350 is working in a not inverting configuration, driven by a piezo ceramic. The piezo throughput must be bidirectional, so, when on TX, an high level signal is brought to the piezo and the OPA350 positive input is protected by a couple of end to end diodes that limit the signal at +-1V max.
I know that bipolar OpAmp input are very sensitive to reverse breakdown current but this is a CMOS, so the question is simple and probably obvious for people more expert than me: should I worry about damage to the OPA350 in this configuration?
Thanks, any help is appreciated.
Alberto