Hi,
The LMP7721 has its inverting input on 8. Pin 7 is marked N/C. As I need a guard ring around the net on pin 8 to help with surface leakage can I connect the guard to pin 7 or should I run it between pins 6 and 7 or between pins 7 and 8? I am using the SOIC part.
i.e. is pin 7 connected to anything inside the package?
Mike