Other Parts Discussed in Thread: LMH6703, LMH730216
Hi,
I'm working with an LMH6703 op-amp (SOIC-8 configuration) and am having some issues. I'm new to high speed/current feedback amplifiers, so any suggestions anyone can give me would be much appreciated.
I have a 10 MHz signal (coming from a crystal, at about 3V amplitude). This signal is actually coming from another circuit, so I need to apply a buffer, or even 2V/V amplification so that I can rectify the signal for AM demodulation. I have tried just about every configuration of the op-amps that I can think of, including the suggested circuits in the application section of the LMH6703 datasheet (both inverting and non-inverting).
I have tried different configurations with the shutdown pin (pin 8), applying ground, +2.5 V, and letting it float. Applying ground seems to work as it should, as far as causing the op-amp to go into "shutdown mode", and making every input high impedance. However, letting it float and applying +2.5 V (which should "activate" the op-amp) causes some weird effects. For one thing, when I measure the input impedance (with a simple multimeter) between the inverting and non-inverting inputs, the non-inverting impedance is 8 kOhm - 20 kOhm (varying between several different LMH6703's), where it should be 1 MOhm. The inverting impedance is really strange. When I hook up my multimeter, it flashes between OL (inf. impedance) and another value (it happens too quickly to actually give me a number though).
At this point I'm really lost as to what to do. The only hints I've gotten so far is that sometimes I'll see ringing at ~3-100 MHz at the output. Right now, however, I'm seeing absolutely nothing at the output. I've got everything grounded really well. The only thing I'm doing "wrong", is that in the application section of the datasheet, it specifies a 6.8 uf one-way capacitor between ground and the power-rails, I'm currently using a 1 uf capacitor because we don't have any 6.8 uf caps laying around, but I can't see that making a huge difference.
Thanks again for any help. Here's a link to the datasheet:
http://www.ti.com/lit/ds/symlink/lmh6703.pdf
-Adam