I need to build a very sensitive current amplifier for an ion detection system. The detector output current is very low, approximately 100 fA. The required bandwidth is 50 kHz.
The bandwidth implies that a typical transimpedance amplifier will not work. So I'm considering a switched integrator amplifier. Something like the IVC102 is what I have in mind but with a smaller feedback capacitor (e.g. 0.1pF). I have not found an integrated solution like this.
The LMP7721 looks appropriate for a discrete solution given its very low input bias current. In addition, I need a means to discharge the feedback capacitor that has very low leakage current and parasitic capacitance.
Can anyone suggest relevant application notes? How about an appropriate discharge circuit?
Has anyone tried modifying the LMP7721 Multi-function Evaluation Board to work in this configuration?
http://www.ti.com/lit/ug/snou004/snou004.pdf
Does anyone know of an integrated solution like the IVC102 but with much smaller feedback capacitance?
Thanks.
Andy