Other Parts Discussed in Thread: XTR300, XTR300EVM
Hi,
I'd like to use the XTR300 in Current output mode as a V-I converter. Ideally I'd like it to output a constant 1mA independent on the load and the frequency of the input voltage by using Vin=10V and Rset=100k.
I'm trying to characterise the component's behaviour by using the XTR300EVM. Initially I had done load tests tests and am pretty pleased with the results ie there is a clear linear dependency between input voltage and output current and the curves superimpose with 10% error for loads of 1k-10k, this at 10Hz.
However, I'm having difficulty understanding the frequency response. I tried plotting the output current versus the frequency ranging from 1-1000Hz. Although ideally I'm expecting a constant 1mA output, this is only true up to 10Hz. Between 10Hz and 100Hz there is a prominent slope and the values tend to stabilise between 100Hz and 1000Hz at values depending on the load.
eg. for load of 10k the output current drops from 1mA to 0.8mA, for 5.6k the output current increases to 1.45mA and for a load of 2k it increases up to 3.9mA.
Any help on understanding the reason then stabilising the output is much appreciated.
Many thanks,
Hind