This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2903 current at input pin

Other Parts Discussed in Thread: LMC7221, LM2903

Hi,

I'm hoping you can tell me the max current I can feed into the input pins of the LM2903? The LMC7221 for example states that +-5mA is teh max but there is nothing defined for teh LM2903.

 

Cheers

Calum

  • Calum.

    The LM2903 input blocks input current flow up to 30V, so there is no positive (in to DUT) input current.
    If the input(s) go below ground current can flow. The "general rule" of -10mA is certainly safe for the LM2903.
    However, the output state may invert (wrong output) if the inputs go below ground.

    Regards,
    Ron Michallick