I want to make a differential measurement based on two NDIR sensors. I think this is a fairly common practise with NDIR sensors and suspect somebody has already worked this out. At the moment, I have two NDIR sensors, each is connected to its own LMP91050SDEVAL board that is connected to SPIO4 boards which plug into separate USB ports. Both sensors are working separately but I can not figure out how to make the Sensor-AFE-for-91050 software collect when both sensors are connected to USB ports. Apparently the software is only seeing one board, the first USB port it finds. Is there some way to configure the software to set the USB ports so I can collect signals from both sensors? The computer could easily run two copies of the software but I do not see how to set the USB port that is being used for a given copy of the software. In the Device Hardware view I can see both of the NSC_USB boards. Both are assigned to location 0 but have different board ID numbers. There are no error symbols on either USB port.
Another confirguration that we will eventually want to test uses 4 or 5 different sensors. Ideally these would have only one USB port but independent LMP91050s. I wonder if there is a way to link multiple LMP91050SDEVAL boards to a single SPIO4? Do I need to purchase a software development kit to communicate to modules?