Other Parts Discussed in Thread: OPA657, OPA355, OPA656, OPA380
Hi,
I need to design a transimpedance amplifier with gain greater than 10^7 v/A and banwidth greater than 12 KHz .The photodiode capacitance is 75pF & the current signal is in the range of microamps and there are no negative supplies available. I prefer to use the OPA657 in the single supply mode. In the data sheet, it is said that a single supply of +8v to +12v can be used with the negative supply grounded.The dark current output of 0V is not of interest. In this case should I apply a voltage to the non inverting input of OPA657 and can I have the same voltage applied to both + input of OPA657 & the anode of the photo diode? A single to differential converter follows the TIA which has an input commom mode range of 200 mV to 3.9 V with a 5V supply.
Thanks in advance,
Nisha