Other Parts Discussed in Thread: INA333
Hi everyone,
I have recently designed an 8:1 differential analog input circuit making use of an analog differential multiplexer and the INA333.
The schematic is as shown in the attached picture
The INA333 is configured to have a gain of 100.
The differential input signals range from 0 to 50mV.
The interesting problem I have is, if my differential signal goes through the multiplexer(example 30mV), I can measure 30mV on VIN+ & VIN- of INA333. However, the output from my op amp is 60mV instead of the 3V.
When I removed the multiplexer and had 30mV differential voltage source applied directly on the VIN+ & VIN-, I can get 3V.
There seems to be nothing wrong with the multiplexer nor the INA333. Could anyone advise me on this issue? Is there some impedence issue that I am missing out on somewhere?
Hope to have your adivse soon. Thank you.