This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Mechanical Data - INA321

which means what's inside the circles? 

Source: http://www.ti.com/lit/ds/symlink/ina321.pdf

..

  • Hello LaunchRed,

    The most common dimension you will come across are like those in 2, 4, 6, 8, and 10.  These represent the indicated distance and the tolerance.  The number on the bottom is the minimum and the number on the top is the maximum value.  Circles 1 and 5 depict basic dimensions, which is theoretically an exact value.  Circle 9 shows that the height is a maximum of 1.1mm.  I am unsure of what the symbols  mean in 3 and 7.  Perhaps there are websites that discuss mechanical dimensioning symbols. 

  • Very Goood!!! :D