Other Parts Discussed in Thread: LMH6515, THS4304
I build up a schematic with LMH6515 as VGA shown below.
The opamp in this figure is THS4304. LMH6515 Pin13 is connectted to Pin16, so that its output impedance is 200ohm.
When I measured this design, I got lots of problem.
1. VGA(LMH6515) output pins has different DC level. Pin 15 is 2.1V, and Pin 14 is 2.5V, however, they are designed to be 2.8V.
2. The VGA seems have a dynamic range around 50dB. The input signal is 50MHz.
| Input power -20dBm | ||
| Output Power | ||
| Gain Code | Designed | Measured |
| 00000 | -44dBm | -59.87dBm |
| 00001 | -43dBm | -58.72dBm |
| 00010 | -42dBm | -50.61dBm |
| 00100 | -40dBm | -48.81dBm |
| 01000 | -36dBm | -36.63dBm |
| 10000 | -28dBm | -26.46dBm |
| 11000 | -20dBm | -16.99dBm |
| 11100 | -16dBm | -12.79dBm |
| 11110 | -14dBm | -10.73dBm |
| 11111 | -13dBm | -9.52dBm |
3. When the Gain code is set to 111xx, I got lots of spurs. The max one is at 73.7MHz.
4. Even I shut down input signal, I also got spurs.
Does that mean the VGA is unstable? If yes, any suggesttion for the schematic/PCB design?