Other Parts Discussed in Thread: OPA549, INA146
Hello,
I'd like to design a voltage-to-current amplifier to drive current in a near purely inductive load (say L approx 5 uH, R 0.5 - 2 Ohm). I have design an amp using the master-slave configuration in Fig. 14 from the datasheet and that seems to work out well. Now I'd like to switch to a single-supply design (but output needs to swing positive and negative), so I was playing with bridge configurations. I have not been very succesful with that. While I was able to get voltage amps to work okay, driving a current and controlling feedback via a current sense resistor has miserably failed. Has anybody used the OPA549 in this kind of application before ? A reference design would be awesome.
Thank you so much in advance,
Thomas