Everyone,
I'm trying to built a ECG amplifier using INA2126P it is a dual pin configuration and the input is 5mVPP I have built the basic circuit, in order to get the gain 1000 I kept Rg as 80 and also gave the power supply as +/- 5V to both positive and also negative. the output I'm getting is in microV can anybody please tell me what I need to do in order to get proper output. In the specification detail it is said that we need to add extra sense connection I dint get that point, what kind of sensing should be done.0820.ina2126.pdf
I have also kept load resistor as 25Kohm
I'm a grad student not so perfect in designing but any help is appreciated.
I have attached the specification sheet for INA2126P
Thanks in advance
Tejaswi