Here is my design: the differential input pins V+ is connected to previous stage's output; and V- is connected to a VCM=1.4V, which is a AC ground. In my application, the input of the VGA must be DC couple. Then there is a problem: the previous stages may generate DC offset, so the DC voltage of the V+ may differ from VCM. Then I found if the input offset=20mV, the circuit functions is still ok. But if the input offset is increased to 70mV, the circuit stops function properly.
So, my question is: how much input DC offset is acceptable to ensure the circuit funtion properly.