This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dual channel cro adaptor

The circuit is functioning properly with each channel has its own shift and amplifier and a sync pulse of 8 volts

for 0.5uS in the output to work on CROS with no sync input.

 

*1 It was viewed that the circuit only works if the time-base is a multiple of the incoming frequency.So in other

words if there is no variable time base ,then the display won,t be 'streamed' and show the spaces inbeween

the waveforms.

 

*2 If two waveforms are guarranteed to be displayed , the ocilloscope must only display ONE sync pulse on the

start of the screen.Then the frequency multiple is correct and the circuit has to display the two waveforms as

a continuous stream.

 

*3 I'm still confuessed why, as explained in *1, why many waveforms arn't able to be displayed as easily.

The next option is to have a delay between the start of the two waveforms in order to get the frequency

multiple to divide by two.

 

Thanks -Simon