Other Parts Discussed in Thread: INA128
Hi, I'm attempting to use an INA128 in a load cell instrumentation application. I have been successful at setting a gain that will deliver a reasonable range of voltage response, but the problem I am having is that the sensitivity of the load cell on the low end doesn't seem to be where I would like it. In example, adding one gram of weight to the load cell will provide ~3mV of change in voltage. This is the best I have been able to achieve while adjusting gain values. I need a larger value, as the micro-controller I'm using can only sense as low as 5mV increments. The load cell I believe is balanced and to be hooked directly into the sense +/- inputs. My input voltage is 5V, and reference is 2.5V. Excitation voltage is 5V.
My ultimate goal is to amplify this load cell to allow a resolution of 0.5g reading and therefore need to successfully implement this amplifier or similar to allow this with the use of a microcontoller /ADC for further tasks.
Thanks for any insight provided!
Jake