Other Parts Discussed in Thread: LM7121, MAX232
Hello friends,
We have a design which implies two cascaded LM7121, each one configured as non-inverters, G=4...5 and powered by +/-9Vdc.
The input stage is DC coupled from a PI filter LPF and in the very front, there is a balun transformer, so first amp see's ground on positive input.
The question is what if negative supply is some kind different from positive one which is well regulated at +9Vdc. In fact, we steel power from MAX232's available on board as negative rail which is obvious un-regulated and in range of -8...-10Vdc depending on loading. We downloaded spice model for LM7121 and simulations looks very nice but just to be sure. This supposed to be a very flat amplifier in 0.1...10MHz range.
Thanks in advance,