Other Parts Discussed in Thread: INA333
Hi,
I connected the Resistor (1K SMD 1%) between the 1st and 8th pin of the INA333. Ref pin is connected to ground and supply voltage is +5 Volt and Ground. I suppose to get 100 times gain. but i am getting 2 times and it is non linear . like when i give 10mV input. output is 20mV. when i/p is 200mV o/p is 420mV.when i/p is 1.2V the o/p is 3.4V and when i/p is 1.5V the output is 5V. i am not able get any of gain except G=2 even after i changed the resistor from 1K to 100E. can any body help me to solve the problem?. My project is Related to PT100 temperature sensing.