Other Parts Discussed in Thread: OPA693
I would like to know if I can use the OPA693, package SOT-23, instead the package SO-8 for output two video signals with Gain+2 with double power +5V and -5V.
Thanks.
Maria Fey
DSE
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Maria,
The only issue should be related to thermals. The SOT23 package in the datasheet specifies 150 degC/W. The power dissipation can be roughly estimated as shown on page 21 of the datasheet. For 2 video loads the equivalent resistance is 75-ohms. Also, in general, the RMS output current for video is around 8mA/load and around 1Vrms at the amplifier output (always a function of true video signal but these get you in the ballpark).
So Quiescent power lets say is 10V x 14.1mA = 141mW. Video power dissipation in the amp driving 2 video loads is roughly (5V - 1V)*(8mA x 2 loads) = 64mW. For a rough total of around 205mW. With 150 degC/W, the silicon temperature rise is 150x0.205 = 31 degC + Tambient.
With Tambient = 85C, the junction temp would be 85+31 = 116 deg C. It is preferred to keep the silicon junction temperature below 130degC, but can support up to 150degC. Either way this should not be an issue.
Cheers,
Randy