Other Parts Discussed in Thread: DAC0800, DAC0808, XTR116, ISO7641FC, DAC7311, ISO1541, DAC7571
I have an application which need to convert a binary value 0-255 to a 4-20 mA signal. I would like to do this using a XTR116 and DAC0808 or DAC0800 d/a converter. I understand that the XTR requires all current pulled from Vs/Vreg to return to Iret. Can I power the DAC08 from the XTR and have the DAC's output drive the XTR's input while the DAC takes its data input signals (bits 0-7) from a different circuit?
Any advice is much appreciated. Thank you and happy Thanksgiving!