This is sort of a strange question and I think I could hazard a guess from the parameters given in the data sheet, but I think I might get a better answer fom someone more familiar with the part and it's packaging.
We are using the LMC6001AIN in a battery powered application, so the total time it's on is important. The unit is powered from +/-5V with the input connected to ground (0V) during the turn-on time. The ground is removed during measurements. The unit is in an enclosed case (no air flow) and is normally operated at room temperature.
What we are seeing appears to be a slight shift in the offset during wram-up. After warm-up, the unit seems very stable. My question is: What minimum time should we use to allow the amplifier to come to thermal equilibrium?
Thanks