Other Parts Discussed in Thread: INA139
Hi
I want to sum current measurements from few sources Can I use multiple INA139 units and parallel the output currents on one resistor?
Thaks,
Dror
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Dror,
Yes, this is acceptable and the currents will sum as expected. It is recommended to place a small-signal diode in series with each of the outputs in this configuration to ensure that reverse current never flows back into one of the other devices, even if they are powered down or inactive. I would also recommend a small series resistors (100 Ohms) between the summing point for extra protection. Just be sure that the total current into the load resistor doesn't create a voltage potential that is greater than the compliance voltages of the current sources.
Figure 5 shows two units that have shared outputs and a 10kOhm resistor to isolate them. As mentioned a lower resistor value such as 100Ohms can be used. The comparator was only for the bidirectional current sensing scheme shown and would not be needed in your application.